Hello,
We are planning on applying the DLP9500UV into a laser system (COMPEX300 - manual attached) to project larger scaled images. However, the wavelength of the current laser system is 351 nm, which is slightly lower than the specified wavelength range of the DLP9500UV (363nm to 420nm). Is it possible to use it with this laser anyways?
Also, what is the power threshold of the DLP9500UV? As in we would like to know the maximum allowable power that would not cause damage to the micromirrors in the chipset?
Thank you
HN