This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRNANOEVM: Free offer to DLP® NIRscan™ Nano evaluation module users. Determine composition of fabrics using your Nano.

Part Number: DLPNIRNANOEVM


Sagitto is seeking new demonstration applications for its system, so we're making the following offer to all DLP® NIRscan™ Nano evaluation module users :-

  • Register on the Sagitto website and - once you're registered, - request access to the free Sagitto Demonstration Account. We'll automatically give you an initial 200 credits that will allow you to use your  DLP NIRscan Nano to experiment with Sagitto's existing demonstration models, such as the Fabric model. That's enough to test the composition of 20 fabrics, as in the example reports.

  • After trying the Fabric model, if you have application that you think would make a good demonstration of the DLP® NIRscan™ Nano's capabilitiy, and we decide to add it to our list of demonstration models so that other Nano users can try it too, then we'll give you a free Explorer Account (normally US$500). That means you'll also receive a free case for the DLP® NIRscan™ Nano evaluation module ('EVM') to not only protect the electronic circuitry, but also to provide stability during use. We will also send you a free small block of high-quality sintered teflon NIR reflective material.

Regards

George Hill

Note: to use the Sagitto demonstration models, you just need .csv data files created by the TI GUI application - you don't need to use the Sagitto iOS app. Some of the Sagitto demonstration models are not suitable for the NIRscan Nano (see our Whats The Difference explanation here.)

Fabrics - Chinese.pdf

FabricsRegression-brown cloth.pdf