This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010: is color mode and fps/hz set on the chip on the ribbon cable, or the DLPController chip on the board?

Part Number: DLP2010
Other Parts Discussed in Thread: DLPC3430

Is color mode and fps/hz (firmware) set on the chip on the ribbon cable, or the DLPController chip on the PCB?

Reason I am asking is I want to know if I can use the Lightcrafter 2010 to update firmwares of optical engines which also uses the DLP2010 DMD but the board is not designed for monochrome operation mode by default