Other Parts Discussed in Thread: DLP2010
Hello,
I am currently working on building a projection system based on a DMD, and this evaluation board seems fitting for my application. There is just one issue, I need to illuminate at specific wavelengths (565 and 730). So, I was wondering if the best option is to buy this module and somehow deactivate the built-in LEDs, and instead use other LEDs with the wavelengths I mentioned. Or, is there a better option, like buying the DMD separately and building from there?
Thanks a lot!