Hi,
Can the DLPC6401 controller be able to digitally adjust the horizontal keystone (-40 ° to + 40 °, in 1 ° increments) and the vertical keystone (-25 ° to + 25 ° in 1 ° increments)?
If not, is there another controller that can do it?
Best regards,
Michel Da Silva