Other Parts Discussed in Thread: DLP4500
Hello,
We purchased a DLP® LightCrafter™ Evaluation Module (www.ti.com/.../dlplightcrafter) as a projector for our clinic, but we face an issue when we use it to project our generated pattern. We use Matlab to generate a multicolor square pattern as guards to detect the distance between certain objects, the problem is, no matter how we alter the size of our pattern image, the squares change into rectangles after the projecting. In the description, it says that this can display image up to 854*480 and can use patterns resolution of 608*684, but we tried both resolutions, our image still gets a little bit deformation.
I want to ask about the ideal resolution for this projector to display an image that will cause no deformation.
Thanks