This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC2607: Missing portions of the DLPC2607 Datasheet

Part Number: DLPC2607
Other Parts Discussed in Thread: DLPA1000, DLP2000,

We are designing a system utilizing the DLPC2607/DLPA1000/DLP2000, and it looks like the DMPC2607 datasheet does not include any documentation on the D0-D14 pins or the LOADB/SCTRL/TRC/DAD_BUS/DAD_STRB ect... 

There are no ball numbers or descriptions, however, there are references to them in section 6.14 DMD Interface Timing Requirements.

Where can I get a datasheet that is complete and is not missing information about the pinouts?