Hi, I'm an Optical Engineer working on the Illumination optics design for a client. I received a document about DMD Etendue for DLP470TP. (DMDEtendue) from my client.
I need to get some confirmation base on the information provided from the Document (refer to attachment)
Q1. The illumination rays after passing through illumination optics. The rays should be in collimated (parallel) or converging with 17degree light cone) when hitting DMD surface?
Q2. Understand that Illumination ray need to enter with 34degree of Flat state DMD. If 17 degree light cone required, the light enter direction still need to be 34degree, is that correct?