Hi
Currently we using a DMD to verify/test our DLP controller board in SMT workshop. I think this solution is an inefficient and also is easy to damage the DMD.
Is there any other solutions to test DLP controller?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Currently we using a DMD to verify/test our DLP controller board in SMT workshop. I think this solution is an inefficient and also is easy to damage the DMD.
Is there any other solutions to test DLP controller?
Hi qinghua,
Welcome to e2e forum and Thanks for showing your interest in DLP Technology.
Please check the power sequence of DLPC as mentioned in datasheet :
refer to Figure 2, Figure 3, and Figure 16 timing as shown below –
Make sure the PWRGOOD getting asserted only after above core voltages are stable and after asserting POSENSE signal to the controller.
Once you confirm the power-up sequence is good.
Next step is keep the system in boothold (put jumper j26 ) and connect the JTAG to program bootloader.
Once you are successfully able to program boot loader next step is get the DLP ComposerTM lite version to program the firmware.
After successfully upload firmware, you can see heartbeat LED to verify the system is good.
Then you can connect DMD to check final image on DMD.
Thanks,
Navneet