Other Parts Discussed in Thread: DLPLCR65NEVM,
Hi all,
I had some questions about the control software of DLPLCRC410EVM +DLPLCR65NEVM.
1. Test pattern. I can not use the internal test pattern after loading some pictures, even if I tick the test pattern enable box from the test patterns menu. How can I make the test pattern work again? Or do I need to do other things after tick the enable box?
2. Loop in control command. I choose the 'loop ' function to work. But a run-time error: 381 occurred, and then the program closed automatically. I think maybe the order of the script is wrong, but I have no idea about the right script.
3. .bin file loading. I tried to load the test D4100_GUI_FPGA.bin from the GUI, but a run-time error: 481 occurred.
4. Labview support. Can I use labview to control this product? If yes, where I can get the labview kit.
Thanks.
Mei