Other Parts Discussed in Thread: DLPLCR65NEVM,
Hi all,
I had some questions about DLPLCRC410EVM+ DLPLCR65NEVM.
1. As the hinge-axis orientation is 45°, so the horizontal incident light will be positioned diagonally relative to the overall array, reflecting in tilt upward and tilt down according to ‘ON’ and 'OFF' state. Do you have any suggestions about how to mount the DMD to make the reflect light only reflect in horizontal plane without flying up and down?
2.When I stop the running patterns, and after loosing the SW3 button, I still can see the previous running pattern on the DMD, is this right?
Thanks,
Mei