Other Parts Discussed in Thread: DLP5500,
E2E,
I'm working on establishing JTAG tests for a board through a DLPC200 controlling the relevant DLP5500. Scouring the internet resources, the BSDL file/TXT file is conspicuously absent in the series of DLPC. I'm wondering if there's a significant reason for this, if the TI team can provide the BSDL for DLPC200, or if it can be made.
It may also be the case that this device's BSDL may exist from Xilink, but then the file would need to be modified for the TI ZEW BGA 780 pinout.
If this question belongs elsewhere please move it.
Thank you,
T