Other Parts Discussed in Thread: DLPC410
Dear All,
In our early development phase DLPC910 will be driving with 200MHz DCLKIN speed. Does this become any issue?
Thank you and best regards,
Rossinag
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Rossinag,
The device was only tested at the speeds listed in the data sheet, so the 200 MHz clock presents a risk. The PLL design for the input clock is different than the DLPC410 which allows 200 - 400 Mhz. The DLPC910 was designed for 400 MHz or 480 MHz.
It may run at 200 MHz, but there is no guarantee.
FIzix