Hi,
We are using DLPC6401 in the Design.
There is no information on voltage/current for pin "EXRES". Just given 1% resistor.
We have connected 160Ohm 1% resistor with 0.05W(0201 package) for EXRES. Please confirm the power rating is good enough for this. We are de-rating resistors by 50%. so please confirm if the power dissipation is more than 0.025W.
Thanks & Regards
Kranthi