Hello,
I was wondering if it is possible to build a custom firmware desabling gamma correction in video mode? I want to reproduce the effect of I2C "Gamma correction" command (0x31|0x80, 0x00), is there a parameters allowing to do it in the ".ini" file? Maybe "MACHINE_DATA.COLORPROFILE_0_BRILLIANTCOLORLOOK"? I could not find any information on it...
Best regards,