I saw on your website that you have fast solutions, like DLP7000, which can reach a rate up to 32kHz, which refers to the overall refresh rate of the DLP.
In my application, a high spatial resolution along both x and y axis is not mandatory, but it is enough to have a high number of pixels only along one direction.
I saw from the datasheet of DLP7000 that many DMD operations are possible: single block, dual block, ...
I was wondering if it is possibile tu use only a bank of the dmd (letting all the others off) to increase the frame rate at the expense of a lower effective number of rows. Is it possibile in this case to reach 32*16kHz rate with a single bank active?
If not, is there any other possibility to increase the frame rate at the expense of spatial resolution?
Finally, is it possible to increase speed using only a portion of the DMD also with others chips of the DLP family, like DLP5500 or DLP4500?
Thank you for your time
Best regards,
Alessandro Cominelli