Other Parts Discussed in Thread: DLP660TE
Hi, I want to know if there is any possibility to adapt the LightCrafter to 4K DLP660TE DMD. I am planning to use it with UV light source from 365 to 405 nm. If possible, the optics of the system also must be redefined to achieve the desired resolution and use under UV light condition. In case LightCrafter cannot be adapted, can I use DLP660TE EVM kit to develop a customized projector with the same characteristics? It is not clear to me if DLP660TE DMD are prepared for UV light projection. Thank you.