Dear all,
I have a working solution of displaying a set of flash images in Trigger mode 1 with internal generated trigger (see Standard.ini). Firmware version is 4.0.3.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/94/Standard.ini
I changed this solution for external trigger with TRIG_IN_2 in the following way: First pattern with external positive trigger, following patterns without trigger (see Standard - ExtTrigger.ini).
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/94/Standard-_2D00_-ExtTrigger.ini
Now I start the sequence in the GUI. After this I generate the external trigger signal (TRIG_IN_2 goes from Low to High - as seen in the PeripheralControl section of the GUI). But now the patterns were not displayed.
We try external trigger with only one pattern - doesn't work, too.
We try another firmware version (3.0, 3.1.0) - doesn't work, too.
Is there anything wrong with the solution for the external trigger?