Hi TI,
I tried several time to install DLPC4422GUI using, for example, the link below:
http://www.ti.com/tool/DLPC4422-SW
The file is downloading without problem and I can launch the installation (screenshot below).
Sadly, each time I clicked next, the installation stopped and displayed the following error message:
In addition, my antivirus (Avira), signaled an HEUR virus and promptly put the file in quarantine.
Have you ever encounter this problem ?
Do you think it is coming from my antivirus or from the file ?
Regards,