Other Parts Discussed in Thread: DLP2000
Hi,
I am newbie actually can u please guide how to resize projection angle and what is the command for that and also how to project the image perpendicular in DLP.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Prabhu ram,
Welcome to E2E forums! Have you looked at the DLP2000 EVM users guide and the controller Software programmers guide? These 2 documents generally contains all the information regarding the available features.
Thanks & Regards, Hirak
Hi,
Actually i looked into that my doubt is how to reduce the focus are as i seen in that document it doesn't contains about that. And also i need to know how to provide the i2c command to control the projector for example the uploaded image is the address how i need to execute this command can you please elaborate about this.[quote user="Hirak Biswas"]
Hi Prabhu ram,
Welcome to E2E forums! Have you looked at the DLP2000 EVM users guide and the controller Software programmers guide? These 2 documents generally contains all the information regarding the available features.
Thanks & Regards, Hirak
Hi Prabhuram,
Could you please help me understand "- how to reduce the focus " and to resize projection angle?
Are you trying to create a smaller size image at the same distance?
If yes, then it is not a feature of function of the controller or DMD. The throw ratio (Image size at certain distance) is defined by the optics. The optrical engine used in DLP2000 EVM does have have zoom capability, only way to change size of image is by moving the EVM.
regards,
Vivek
Thank you so much for your valuable reply and i have another doubt how to change the projection area (suppose it is projecting in the wall means i need to project the same in projector placed surface) Is this possible
Hello Prabhuram,
Could you please further elaborate your question. It is not clear to me what do you want to change?
regards,
Vivek
My question is how to project in the surface of the projector placed area like Xperia projector is it possible