The ID read from dlp4710 is 60d 00 8A. According to the description in section 2.3.3.73 of dlpu035 manual, the ID is 60d 00 68,
which is inconsistent with the actual situation, and there is no such item in the manual.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The ID read from dlp4710 is 60d 00 8A. According to the description in section 2.3.3.73 of dlpu035 manual, the ID is 60d 00 68,
which is inconsistent with the actual situation, and there is no such item in the manual.
Hello,
One of the original device IDs for the DLP4710 was 0x60 0D 00 6B. However, one of the updated fuse IDs is 0x60 0D 00 8A. In either case these device IDs are correct for the DLP4710.
Thanks,
Kyle