Other Parts Discussed in Thread: DLP660TE
Hello, TI.
I have a question from Korea.
We purchased DLPDLCR660TEVM products through TI.
I'm doing a test one by one, looking at the guide, and there are a few problems.
The first problem is that the switch button on the DLP board is reversed.
The second problem is that I can float a test pattern, but I wonder how I can use the binary image I want to use.
Do you have any more links or guides to refer to? Or I wonder if there's a place to get the coding.
I wonder what external input should be done if external input mode is used.
I wonder how the 4422 board uses the V by one and how the 9 pin d-sub works.
Thank you.