Other Parts Discussed in Thread: DLP650LNIR, DLPC410, DLPLCR65NEVM
Has any of the DMDs been released with NIR or NIR2 window?
I see DLP700 and DLP7000UV, for example, but DLP7000NIR is nowhere to find.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Has any of the DMDs been released with NIR or NIR2 window?
I see DLP700 and DLP7000UV, for example, but DLP7000NIR is nowhere to find.
Thanks.
Hello Laszlo,
First, welcome to the DLP section of the TI E2E community.
We do not have a DLP7000NIR.but we do have a DLP650LNIR which is similar. It is supported by the DLPC410 but the PROM must be DLPR410AYVA. The earlier PROM DLPR410YVA will NOT recognize the DLP650LNIR.
The EVM's are now divided up so that you can get a DMD board [DLPLCR65NEVM] and Controller board [DLPLCRC410EVM] separately.
If you are used to working with the DLPC410 kit, It will be quite familiar
Fizix
Great!
Thanks Fizix.
Do you know if Ti plans to release the full-HD version (2048x1080) with NIR coated window?
Laszlo
Hello Laszlo,
I am not aware of any specific plans for a 1080p NIR device. Depending on the reception of the DLP650LNIR.we may consider other NIR chips.
Fizix