Hi,
I am studying DLP3030PGUQ1EVM as a HUD light source, but the user's guide contains less information.
Can someone help my questions below:
1. What is the dimension of the PGU?
2. What is the active area of the PGU?
3. What is the view angle (or chief ray angle) from the diffuser?
4. Can I have projection lens layout information in the PGU?
5. Can I control the movement of this unit using a stepper motor to adjust the location of image displayed on the windshield of a car?
Here is the reference design: http://www.ti.com/solution/head-up-display-hud?variantid=22362&subsystemid=24904