Other Parts Discussed in Thread: DLP3010EVM-LC
I am using the DLP3010LC GUI, version 2.2.0.6. I am trying to make an updated flash image, that contains some new internal patterns.
I have gone through the steps to create a pattern binary, that I have saved to file.
I have gone through the steps in the "Firmware" section, in order to Update Flash Image. I am using the base firmware input called dlp3010evm-lc_7.3.2.img
As I go through the final step and push "Finish", I get the following error code:
"Flash Builder returned with error code 12"
The GUI does say that "Flash Image Update Completed", but no output is written to file.
I have tried various options searching for something that does not give the error, but I have not been successful.
So my questions:
* What does error code 12 mean?
* How can I avoid it?