This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC6401: GUI and firmware

Part Number: DLPC6401

Hello,

I am designing a DLP control board with the DLPC6401. In various documents and posts, I see the DLPC6401 GUI tool mentioned. However, I cannot find a download link. Can you provide me with the download?

Also, I am unclear on the firmware requirements.

  • Is the USB connection needed or can I do everything over I2C?
  • Can I flash the boom ROM via the DLPC6401 or do I have to program it manually?
  • Where can I find an image for the boot ROM? Does TI provide it, or should I ask my optical module manufacturer?

Thank you in advance,

Kind regards,

Jim