This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: DLP4710EVM-LC longer exposure time

Part Number: DLP4710EVM-LC


Dear Sir,

we had also purchased the 4710EVM_LC and want to use longger exposure time with external LED Driver.   My situation is same with Mr. Lennart Denecke:

"DLP4710EVM-LC: Set maximum exposur time in internal pattern mode above 18 ms"

our application exposure tme is varied between 5--40ms for different pattern set. in our 4500 DMD, we use variied exposure mode. it works fine.

in DLP3479 and 4710DMD, the work mode is different.  we need to find way how to have find simillar work mode to replace 4500.

Could you also send  me the new firmware to test? currently we still use V7.0.1(Nov 6th, 2019).

Thanks  a lot!

Best Regards!

Eric