This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000: Real time pattern reading

Part Number: DLP9000
Other Parts Discussed in Thread: DLPC910, DLPC900, ,

Using the TI software, we can only preload the patterns into the flash and then display them. Is it possible to load the patterns in real time?

For example, I select a folder from the computer and then start the DMD. Then the DMD will automatically read one image, display it and then read another image, display it...Till it reads and dispalys all the images in the folder.

Thanks!