This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000X: DLP 9000 pattern

Part Number: DLP9000X
Other Parts Discussed in Thread: DLP9000, DLPC900

Dear TI support,

As the DLP9000 includes 2 DLPC900, it is meaning that the DLP9000 EVM is capable of 2x400  1-bit binary compressed patterns. Am I right?  And what is the load time for 540 imges?

Thank you.

BR,

Jing Xia

  • Hello Jing Xia,

    When running the DLP9000 DMD with 2 DLPC900 Controllers, the DLP9000 DMD is capable of displaying up to 9523 1-bit binary patterns per second, 1031 8-bit grayscale patterns per second (preloaded with illumination modulation), and 360 8-bit binary patterns per second (external video input).

    To answer your load time question, can you please describe what type of images you are loading? Are they 8-bit, 1-bit, pre-loaded, external loaded, etc?

    Regards,

    MM

  • Hi MM,

    Sorry to reply late. And it is 1-bit images.

    Thank you.

    BR,

    Jing