Other Parts Discussed in Thread: DLPC910
I am writing to ask the 8-bit gray scale illumination of DLP9000X. I am wondering the meaning of a maximum frequency 1873Hz in 8-bit gray patterns. Does it mean if I set an input picture with 8-bit gray scale, the minimum diaplay time should be 1/1873 second? So the minimum modulation step will be 1/1873/256=0.023 ms? Thanks!