Other Parts Discussed in Thread: DLPC-API, DLPC3479
Hi,
I have a question about DLPC-API's ReadSystemStatus function.
In the DLPC3479 Software Programmer's Manual (P.73), System Status's Byte1 is like below.
The bit(2) of the status is "reserved",
but in DLPC-API, ReadSystemStatus function (DLPC34XX_DUAL_ReadSystemStatus) seems to read the bit(2) as "DmdTrainingError".
Also, the function seems not to read bit(7:3).
Why does the API function read bit(2) and not check bit(3:7)?
Regards,
Goto