This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: mid-wave infrared single pixel imaging system using DMD

Part Number: DLPLCRC410EVM
Other Parts Discussed in Thread: DLPLCR65NEVM,

Hello,

We want to develop an infrared single pixel imaging system using a TI DMD and an IR detector that we have fabricated.

We have two requirements:

1) We need the operating wavelength to be as long as possible.

2) We need the required circuitry/accessories along with the DMD device so that it is as straightforward as possible to implement the system.

Is DLPLCRC410EVM together with DLPLCR65NEVM the best option considering these two requirements? Would DLPLCRC410EVM + DLPLCR65NEVM provide us with everything needed for the DMD to be operated/controlled by a Windows PC?

Thanks a lot,

Nima