Other Parts Discussed in Thread: DLPNIRSCANEVM
Dear Team
Good day!
I need to confirm something details about DLPNIRNANOEVM and DLPNIRSCANEVM with you ,
1. DLP NIRscan use the transmissive head , DLP NIRscan Nano use the reflective head . The customer want to confirm that does the DLP NIRscan Nano only
support the reflective head ? whether can use the transmissive head , is there any reference design or information about the DLP NIRscan Nano use the
transmissive head . or how to transform the DLP NIRscan Nano EVM .
2. For the DLP NIRscan Nano EVM Wavelength Range is 900 - 1700 nm , but the DLP2010NIR can support 700-2500 nm , why the EVM shorten the Wavelength
Range , is the EVM Hardware limitation or software limitation ? if the customer want to expand the Wavelength Range , what should they do ?
Thank you for your help
Best regards,
Leon.liu