Other Parts Discussed in Thread: DLP4500NIR, DLPC350
Hi Team,
Our customer is considering to use the DLP650LNIR in the 2500nm wavelength. They are aware that the DMD was only specified at 2000nm and would like to simulate the transmission tradeoffs at 2500nm. They've noted that the visible coatings on Corning 7056 show ~70% transmission - this kind of transmission is acceptable in their application so they're assuming the DLP650LNIR would also work fine. Would it be possible to get the layer thicknesses of the AR coating for them to simulate the behavior beyond 2000nm?
Thanks!
Kind Regards,
Jejomar