Other Parts Discussed in Thread: DLPC4422,
Hi,everyone
1080P resolution is supported by DLP650NE+dlpc4422 . is it supported 1024*768 or 800*600 or downward standard resolution by DLP650NE+dlpc4422? I read dlp650ne datasheet that is only 1080P
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,everyone
1080P resolution is supported by DLP650NE+dlpc4422 . is it supported 1024*768 or 800*600 or downward standard resolution by DLP650NE+dlpc4422? I read dlp650ne datasheet that is only 1080P
Hello,
Thank you for using the DLP E2E forums.
The DLPC4422 and DLP650NE chipset is only able to support the native resolution of the DMD. In this case, the input source resolution must match the 1080p resolution of the DMD.
However you can utilize a front-end board, that has a scalar, in order to support more resolutions. Just make sure that the output of the front-end board matches the DMD resolution.
Regards,
Oscar