This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3021-Q1: PCB designing help

Part Number: DLP3021-Q1

Hi there,

I am working on a new project with DLP3021-Q1, I wish to get help with PCB design related mounting DLP3021-Q1 module on the PCB. so first may I ask it is possible to provide a PCB file for DLP3021-Q1 System Example Schematic -DLPR059.ZIP ?

Thanks for your time.

Kind Regards

James

  • Hello James,

    Unfortunately we do not yet have a layout file example schematic.  We will have this available when an evaluation module for the DLP3021-Q1 is available which should be late this year.

    If you are wondering about the DMD mounting, have you seen the mounting concept information (DLPC127)? This will have the info needed to make the mounting holes on the PCB.

    Best Regards,

    Jackson