Hello
I am interested in using the DLPLCR70EVM DLP board and the DLPLCRC410 Evaluation Module in a project.
I need to be able to flip individual pixels at a rate higher than 32,225 Hz.
I understand the the maximum frequency at which we can re-write every pixel in the array is 32,225 Hz but is it possible to flip single pixels leaving the bulk of the pattern the same faster than this?
Best regards,
James