Other Parts Discussed in Thread: DLPLCRC410EVM
Hi
I have a DLP650LNIR + DLPLCRC410EVM evaluation module which has been running with no problems when connected to a Windows 7 laptop, used for development.
Now I need to use a Windows 10 machine to ship the unit but the DMD is not being enumerated correctly in Windows 10.
Hardware setup is identical. Running the latest Discovery 4100 GUI software, v2.0 ('dlpc133'). Direct connection, no USB hubs in the way.
Under device manager I have:
Windows 7: Universal Serial Bus Controllers => TI 4100 Explorer
Windows 10: Other devices => DLI USB FX2 Firmware 2008, and the device is flagged as having a problem.
Do I need to point this device at somewhere else?
Thanks