This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR660TEVM: Displaying custom patterns

Part Number: DLPDLCR660TEVM
Other Parts Discussed in Thread: DLPC4422, , DLPLCRDC4422EVM

Hi,

I would like to be able to display custom static patterns on the DMD. I'm using the DLPC4422 GUI. I've seen responses on this board saying that you can do so with DLP composer software, but also that it can be done with an external source with a front-end card that has a V-by-1 interface. For static patterns, which method would be better? In the case of using an external source, how does that work?

Thank you,

Katya