I have a problem writing images to DLP6500.
It has two problems:
1. (I2C write returned < 0, means error)
2. compress image -2 , it means the image is not a 24-bit image, but it is in fact a 24-bit image on my computer)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a problem writing images to DLP6500.
It has two problems:
1. (I2C write returned < 0, means error)
2. compress image -2 , it means the image is not a 24-bit image, but it is in fact a 24-bit image on my computer)
Hello User,
Regarding the 24 bit image, there are a number of formats. Is this a special image or something you could post here for us to try?
Fizix