This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000X: Maximum length from DLPC910 to DLP9000X

Part Number: DLP9000X

I think LVDS data length should be complied within 375mm as datasheet saying. However, I would like  to know the background how is the MAX length decided as 375mm. Are there problems when more length is used?

  • Hello Uryyy,

    This length is because the DLP9000X is designed to run at a faster speed of 480 MHz.  This is the maximum length that TI can guarantee the signal integrity.  It will likely work beyond that length, but is not guaranteed.

    Fizix