I think LVDS data length should be complied within 375mm as datasheet saying. However, I would like to know the background how is the MAX length decided as 375mm. Are there problems when more length is used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I think LVDS data length should be complied within 375mm as datasheet saying. However, I would like to know the background how is the MAX length decided as 375mm. Are there problems when more length is used?
Hello Uryyy,
This length is because the DLP9000X is designed to run at a faster speed of 480 MHz. This is the maximum length that TI can guarantee the signal integrity. It will likely work beyond that length, but is not guaranteed.
Fizix