Other Parts Discussed in Thread: DLPC910
Hello,everyone,
We tryed to drive the DLP9000X DMD,but failed. When I load the data pattern into the dmd,nothing exist on the dmd。
1.ECP2_FINISHED status is correct(High) when I power on our pcb driver board .
2.VLED0 & VLED1 status are correct.
3.I can get DMD_TYPE(3:0) = "1111" and DDC_VERSION(2:0) = "010" through apps fpga debug tool(Xilinx ISE Chipscope)
4. After downloading the apps test file into the apps fpga, I find the RST_ACTIVE's status is not correct(HIGH->LOW,But I didn't load anything into the dmd ).
5. I load the data into dmd(load 1600 row and then global reset ),but nothing on the dmd.
What Can I do next,and How can I debug?
Thank you !