This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5531-Q1: Selection criterion for green wavelength operation

Part Number: DLP5531-Q1
Other Parts Discussed in Thread: DLP5530-Q1, , DLP5534-Q1

Hi I want to know which chip should I use among 5530-Q1,5531-Q1 and  5534-Q1, if I want to illuminated the DMD chip only with green wavelength and 10 W optical power, and use full resolution of 1152x1152 video.

  • Hi Divya,

    To better answer your question, can you share what your use-case and application is? The DLP553x-Q1 devices are typically recommended based on application type:

    • DLP5530-Q1: Automotive Interior Display, such as RGB Head-Up Display
    • DLP5531-Q1: Automotive Exterior Display, such as monochromatic High Resolution Headlight
    • DLP5534-Q1: Automotive Interior Display, such as Transparent Window Display

    Based on the similarity and performance considerations of your application, we can recommend the appropriate DLP chipset.