Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR65NEVM: NIR laser beam with different 2D binary patterns on the DMD

Part Number: DLPLCR65NEVM
Other Parts Discussed in Thread: DLPLCRC410EVM

Hi Team,

Can DLPLCR65NEVM + DLPLCRC410EVM bundle modulate a  NIR laser beam with different 2D binary patterns on the DMD? If not, is there other option can do this?

Thank you

Regards,

Maynard

  • Hello Maynard,

    As long as the two patterns are not overlapping at any point it should be possible to modulate them up to the pattern rate the DMD is capable of.  If this is not what you mean could you further clarify what you mean by "modulate an NIR laser beam with different 2D patterns"?

    Fizix