This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP Product information



Hi TI expert

I m interested in the DLP technology.  I want to create a digital advertising screen on the back windshield of my vehicle.  I am just now trying to figure out what I need to make this happen.  I do know that I need a real projection screen/film to adhere to my back window.  I believe you have this product.  I also need a projection screen that can project onto the projection screen.  DO you have these as well?


Best regards,

Thomas

  • Thomas,

    I know that there are some manufacturers that make a special film that you project deep blue (maybe 405 nm?) that will fluoresce.  This way is fairly good, but may be outside the budget that you have. 

    There are also rear projection screens that you can get the material from (i.e. replacement material) but you would have to make a frame.

    There may be other companies that make a film that adheres directly to the glass.  You will need to search for that.  A quick search shows several companies that make such a film.

    In the case of regular projection (not 405 nm) any consumer projector could work.  It will depend on the venue.  If you wish to project during the day,  then you will need a higher lumen projector.  Most of them are made for a larger screen area, so that if you make the image small enough to fit on the back windshield it may be bright enough.  

    If only at night, you will not need as many lumens. You will have to experiment a bit.

    Ben