Part Number: DLPDLCR4710EVM-G2
Other Parts Discussed in Thread: DLPA100, DLPA3000, DLP4710, DLP3010, DLP2010
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPDLCR4710EVM-G2
Other Parts Discussed in Thread: DLPA100, DLPA3000, DLP4710, DLP3010, DLP2010
Hide-san,
It sounds like you are using the DLP LightCrafter GUI to try to perform the flash write function.
The DLP LightCrafter GUI software is designed to specifically support the DLP EVMs on TI.com (so, the DLP2010, DLP3010, DLP4710, etc.). The software will detect what chipset you are using before performing the flash write. It is likely that you are encountering problems due to the chipset combination you are using with the system, which is not supported with any of our LightCrafter EVMs.
I will reach out to you in a private message to help you with support on this particular chipset.
Best Regards,
Philippe