Hello,
I just installed DLPC230 Control Program and get an error when I launch. The following is the error message:
---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Crash File for DLPC230 Control Program 1.8 Build 1242 (3142475da8d7)
Current Time: 4/12/2021 6:26:21 PM
Message:
4/12/2021 6:26:21 PM
Exception : Could not load file or assembly 'DLPComposer.SDK.Lite.dll' or one of its dependencies. The specified module could not be found.
Source : InterfaceDefinition
TargetSite : Boolean EncryptToFile(System.String, System.String, Common.ContentType, Common.ArchiveType)
Stack Trace :
at InterfaceDefinition.ApplicationManager.EncryptToFile(String FilePath, String Contents, ContentType ContentType, ArchiveType ArchiveType)
at InterfaceDefinition.ApplicationData.PopulateCurrentMode()
at InterfaceDefinition.ApplicationData.FillApplicationDataSettings()
at ControlProgram.MainForm..ctor(String[] Args)
at ControlProgram.ControlProgramApplication.OnCreateMainForm()
at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.OnRun()
at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.DoApplicationModel()
at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.Run(String[] commandLine)
at ControlProgram.Program.Main(String[] args)
Data :
InnerException : null
------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Can anyone help me run the program?