I am looking to change the LED PWM at each step of my sequence in "pattern on the fly" mode. My ideal solution would be to enter a PWM value for each image using the built-in sequencer within the GUI.
The GUI as-is does not seem to support this functionality. I cannot enter PWM values per step and cannot find a way to do so within the GUI itself or from reading the documentation.
Another route would be using a batch file to change the LED PWM and output image one after another then run this as a loop (much like the factory test image loop loaded onto the device).
I am able to change the PWM to various values as part of a batch command, but I am unsure how to set output images this way. If I can figure out the correct batch file command to load an image I think I can produce what I want by interspersing the PWM outputs with image updates.
Any help is appreciated.