Other Parts Discussed in Thread: DLP4711, TIDA-01226, DLPC3439
Hi TI,
I made a new PCBA to attach a DMD (DLP4711) and tested it with my DLP system but it seems that half of the mirrors don't work correctly. The mirror array coordinates which have issue is from (0,0) to (959, 1079).
As a trial check, I replaced it with a PCBA from TI's 4710EVM.
In that case the DMD's mirrors can all display correctly.
I've checked my PCBA pin connections and they all are correct. so I suspect the root cause of the issue belongs to a difference in PCBA's layout pattern.
I would like to compare these layout files to find out the difference but I can't find your PCBA's layout file on your web page TIDA-01226 which stores all technical documents related to 4710EVM. Is it difficult to share the layout file?
The PCBA's P/N number is 00.LH901G001 REV.B.
Its name is FLA7(LH90) Flash board.
I'm looking forward to a good reply.
Regards,
Hide